Technical FAQs

Ask a Question

Will a QO24L70S load center accept a 2-pole QO breaker with a factory installed accessory?

Yes, this load center will accept a QO 2-pole breaker with a factory installed accessory. The accessory module will protrude into the left side gutter space.


CTA-ID : 2006855
Was this helpful?
What can we do to improve the information ?