Technical FAQs

Ask a Question

What is the difference between the QO330M150RB and QO330MQ150RB load centers?

Issue:
Product design features

Product Line:
QO Load Centers

Environment:
Product features

Cause:
Application

Resolution:
The old QO330M150RB Series S01 or S02 is an old, now obsolete load center and the current replacement is the QO330MQ150RB Series S03. The Old load center used a KDL Main Breaker, where the new design load center uses the QDL Main breaker.




 
Was this helpful?
What can we do to improve the information ?