Technical FAQs

Ask a Question

What is the difference between a QO342M200RB and a QO342MQ200RB load center?

Issue:
Product Features

Product Line:
QO LC

Cause:
Clarifying product features differences

Resolution:
The QO342MQ200RB (Series S03) has a new style of main circuit breaker installed. The KDL main circuit breaker supplied in Series S01 or Series S02 panels has been replaced by the QDL main circuit breaker.


CTA-ID : 2006422
Was this helpful?
What can we do to improve the information ?