Technical FAQs

Ask a Question

Is a QO35FM30TTF load center supplied with a factory installed main breaker?

No, the main breaker must be field installed in this load center. Use a QO single pole breaker, 30 ampere maximum (purchase separately).

CTA-ID : 2006844
Was this helpful?
What can we do to improve the information ?