Technical FAQs

Ask a Question

What are the Hvir comet part numbers?

IRHVIR70SW2, IRHVIR80SW3 & IRHVIR100SW4 are the 2`` 3`` & 4`` short wave versions
IRHVIR75LW2, IRHVIR85LW3 & IRHVIR105LW4 are the 2``,3``,4`` long wave versions
Can be purchased by distributors or installed by field services. The selection of short or longwave has to do with the type of camera being used.


CTA-ID : 2006843
Was this helpful?
What can we do to improve the information ?