Technical FAQs

Ask a Question

What is the part number for a line reactor for a 1hp, 460 volt, 3 phase input drive?

The part number is RL00202 for the open style and RL00212 for the enclosed unit.
This reactor is also suitable for se wtih ATV28 575 V. drive


CTA-ID : 2006685
Was this helpful?
What can we do to improve the information ?