Technical FAQs

Ask a Question

What is the difference between a QO342M225 and a QO342MQ225 load center?

Issue:
Product Features

Product Line:
QO LC

Cause:
Clarifying product features differences

Resolution:
The QO342MQ225 (Series S03) has a new style of main circuit breaker installed. The KDL main circuit breaker supplied in Series S01 panels has been replaced by the QDL main circuit breaker. The new style load center requires cover QOC342MQF (flush application) or QOC342MQS (surface application).


CTA-ID : 2006418
Was this helpful?
What can we do to improve the information ?