Technical FAQs

Ask a Question

Customer has the NC361200 breaker and asks what is the adjustment on the face of the breaker for?

This adjusts the magetic trip sensitivity between a minimum if 5000a and a maximum of 10000A short circuit current.

CTA-ID : 2006410
Was this helpful?
What can we do to improve the information ?