Technical FAQs

Ask a Question

When did the 9070 Type T and TF line of industrial control transformers (CPT) replace the 9070 Type K to become Square D`s primary line?

The 9070 Type K transformers were officially replaced by the Type T line in May of 1997.

If the customer has concerns about the mounting dimensions of a Type T versus a Type K, the only units that had any differences are listed in document # 7400PN9701


CTA-ID : 2002891
Was this helpful?
What can we do to improve the information ?