Technical FAQs

Ask a Question

Can a QO816L100DFCU load center be top or bottom fed?

The Main Lugs of this load center are positioned at the top of the load center. The interior cannot be rotated to position the Main Lugs at the bottom of the load center. However, there is adequate gutter space to feed the incoming conductors into the bottom endwall of the enclosure, routing them through the side gutter for terminating into the Main Lugs located at the top of the load center.

CTA-ID : 2006004
Was this helpful?
What can we do to improve the information ?