Technical FAQs

Ask a Question

What are the dimensions of the 9034LSVFW2.

The dimensions for the 9034LSVFW2 are main devise is 4.4 in X 1.9in . the dimension for the forks  is 5 in


Click on link below.


CTA-ID : 2003950
Was this helpful?
What can we do to improve the information ?