Technical FAQs

Ask a Question

Is the aluminum bus for NF and NQOD panel rated 750A per square inch?

Issue:
Is the aluminum bus for NF and NQOD panel rated 750A per square inch?

Product Line:
Panelboards.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
Interior bus is rated according to heat rise testing. Current Density Rated bus can be chosen in Product Selectors.

Revised 3/10/04



CTA-ID : 2005783
Was this helpful?
What can we do to improve the information ?