Technical FAQs

Ask a Question

Are the QO or QOB with the ring tongue option designed and suitable for field connectivity?

They are not suitable for field wiring. The intent is that an OEM wires it in his equipment.

CTA-ID : 2005780
Was this helpful?
What can we do to improve the information ?