Technical FAQs

Ask a Question

What individual mount enclosures are available for a 500Vdc circuit breaker application?

The following enclosures are marked for used with 500Vdc circuit breakers: FA100A, FA100AWK, FA100DS, FA100F, FA100RB and FA100S; KA225A, KA225AWK, KA225DS, KA225F, KA225RB and KA225S; LA400AWK, LA400DS, LA400F, LA400R and LA400S; MA1000AWK, MA1000DS, MA1000F, MA1000R and MA1000S; MA1200S.
NOTE: For 500Vdc applications, special circuit breakers with a DC suffix must be used. Refer to the Supplemental Digest for circuit breaker selection.

CTA-ID : 2005570
Was this helpful?
What can we do to improve the information ?