Technical FAQs

Ask a Question

What is the drawing number for the QO48M30DSGP or QO48M60DSGP Generator Panel?

Issue:
Approval Drawing

Product Line:
QO Generator Panel

Cause:
Approval drawing access

Resolution:
Drawing #3051 is available on-line at www.schneider-electric.com/us.
Link: http://static.schneider-electric.us/docs/Electrical%20Distribution/Load%20Centers/QO%20Three%20Phase%20Load%20Centers/3051.pdf
Drawing #3051 is attached, as well. 


CTA-ID : 2006194
Was this helpful?
What can we do to improve the information ?