Technical FAQs

Ask a Question

What is the operating temperature of 9001SKYP pendant stations?

Issue:
What temperature rating does the 9001SKYP pendant station carry? 

Product Line:
9001SKYP ** polymeric pushbutton enclosures

Environment:
Maintenance/repair parts
 
Resolution:
Operating temperature of the pendant enclosure is restricted to the operating temperature of this push buttons used in the pendant station. This is -13 to +140 degrees F or -25 to +60 degrees C.


 
Was this helpful?
What can we do to improve the information ?