Technical FAQs

Ask a Question

What does the magnetic trip adjustment tolerance of +/-25% on the low setting and +/-20% of the high setting mean?

It will trip within 25% above or below the LOW value. Likewise, it will trip within 20% above or below the HIGH value.

CTA-ID : 2005753
Was this helpful?
What can we do to improve the information ?