Technical FAQs

Ask a Question

Does an LXL36125 come with lugs?

Yes. The standard lug is an AL600LI35 and will accept 2 -- #1 AWG - 350 kcmil cables. It also has 2 optional mechanical lug kits. An AL600LI5 that accepts 2 -- #4/0 AWG - 500 kcmil cables, and an AL600LI7 that accepts 1 -- 500 - 750 kcmil cable.


CTA-ID : 2005751
Was this helpful?
What can we do to improve the information ?