Technical FAQs

Ask a Question

What is the current rating on the DC contacts of the Model 98 Temperature Control module?

The contacts have a 0.5 amp rating at a maximum voltage of 125VDC.


CTA-ID : 2006167
Was this helpful?
What can we do to improve the information ?