Technical FAQs

Ask a Question

What is the maximum altitude at which a Double Throw safety switch can be installed?

The maximum altitude of the site of installation should not exceed 6,600 ft. (2,000 m) per NEMA Standards Publication KS-1,``Enclosed and Miscellaneous Distribution Equipment Switches``.


CTA-ID : 2005986
Was this helpful?
What can we do to improve the information ?