Technical FAQs

Ask a Question

How do I get a Masterpact MP or NW/NT fungus treated?

MASTERPACT circuit breakers comply with T2 tropicalization (IEC Standard 68-2-30); relative humidity 95% at 113F (45C) and 80% at 131F (55C) (hot, humid climate). Salt spray resistance as per IEC 68-2-11.
Additional fungus treatment is not necessary.

CTA-ID : 2005978
Was this helpful?
What can we do to improve the information ?