Technical FAQs

Ask a Question

Who provides support for Class 6522 Bubbler / LevelPak or 6524 Programmer devices.

These devices were used to monitor and control the fluid level and pump sequencing in a process. The programmer would monitor the actual level, compare it to conditions programmed on its cards using potentiometers, and used discrete / analog (optional) signals to run electromechanical starters or drives.

These devices were obsoleted in the late 1980s and there is no support for them. User`s may be able to replace the system using a small PLC. The local Applied Product Sales person should be contacted to review the application and offer a solution.


CTA-ID : 2005741
Was this helpful?
What can we do to improve the information ?