Technical FAQs

Ask a Question

Are knockouts provided in the QOM2E2200NRB enclosure?

Issue:
Product Features

Product Line:
Circuit Breaker Enclosures

Environment:
Enclosure Knockouts

Cause:
Installation

Resolution:

The QOM2E2200NRB consists of a QOM2200VH circuit breaker mounted in a QOM22225NRB enclosure. Knockouts are provided in the enclosure. Refer to Drawing #3139 for more detailed knockout information.


CTA-ID : 2004955
Was this helpful?
What can we do to improve the information ?