Technical FAQs

Ask a Question

Is there a 50 amp breaker for use in an MP42200?

No, this device uses the QOM2-MM circuit breakers, available from 100 ampere through 200 ampere.


CTA-ID : 2005521
Was this helpful?
What can we do to improve the information ?