Technical FAQs

Ask a Question

What is the max temperature rating of a 9037HW30.

Min is -30 degrees C, Max is 105 degrees C. Note that there is an error in Digest 172, pg. 20-28.


CTA-ID : 2006154
Was this helpful?
What can we do to improve the information ?