Technical FAQs

Ask a Question

An older QMB panel with 2 QMB3660 switches has 1 with operating handle on left and the other with operating handle on the right. He needs to replace one switch with the other but the load lines are on the wrong side. What can he do?

The spare switch can be flipped over so that the lugs are orientated as needed. The switches were made so that the line and load could be alternated.

CTA-ID : 2005507
Was this helpful?
What can we do to improve the information ?