Technical FAQs

Ask a Question

Is the fuse holder considered field replaceable in a QMB222TW switch?

Only the parts listed below are field replaceable in a QMB222TW twin switch:
Load base assembly P/N 40560-026-50 (Includes lugs and clips). There is one base per switch unit (two units per switch assembly).
Arc Shield /Suppressor Assembly P/N 40512-534-50. One per switch unit.
Handle Knob Kit P/N 40283-437-50.
Lug Assembly (Per Lug) P/N 40251-016-52

CTA-ID : 2006150
Was this helpful?
What can we do to improve the information ?