Technical FAQs

Ask a Question

Can the solid state overload relay be provided on the Class 8941duplex controllers?

As a basic rule SSOLR H-Forms apply to all Class 8536, 8736, 8538, 8539, 8738, 8739, 8810, 8940 (NEMA Style), 8606, 8630, and 8941 controllers.


CTA-ID : 2003480
Was this helpful?
What can we do to improve the information ?