Technical FAQs

Ask a Question

Can a QO330M200, Series S01, load center be bottom fed?

Yes, this load center can be modified in the field for bottom Main Breaker positioning. First, rotate the main breaker 180 degrees, then rotate the entire load center 180 degrees.


CTA-ID : 2005954
Was this helpful?
What can we do to improve the information ?