Technical FAQs

Ask a Question

Can a QO330M200RB, Series S01 or S02, load center be bottom fed?

The Main Breaker of this rainproof load center is positioned at the top of the load center. The interior cannot be rotated to position the Main Breaker at the bottom of the load center. However, there is adequate gutter space to feed the incoming conductors into the bottom endwall of the enclosure, routing them through the side gutter for terminating into the Main Breaker located at the top of the load center.


CTA-ID : 2005948
Was this helpful?
What can we do to improve the information ?