Technical FAQs

Ask a Question

Can a QO327M100RB, Series S01 or S02, load center be top or bottom fed?

The QO3100VH Main Breaker of this load center is branch mounted in the top, left branch position. It cannot be repositioned to another location. The feed can be made from the top or bottom.

CTA-ID : 2005944
Was this helpful?
What can we do to improve the information ?