Technical FAQs

Ask a Question

Are the the lamps for our light modules UL listed?

It is not standard practice to put UL listing on lamps. Lamps are tested with a device and listed under the devices UL listing as long as the perimeters for the lamps wattage requirements are met.

CTA-ID : 2005935
Was this helpful?
What can we do to improve the information ?