Technical FAQs

Ask a Question

What is the interrupting rating of the NHF361200 breaker?

1984 and later Digests list NH at 100k @ 240 and 50k @ 480

1982 and 1981 Digest lists NH at 65K @ 240V and 50K @ 480V.

1980 and earlier digests list the NH at 65K @ 240V and 35K @ 480V.


CTA-ID : 2005717
Was this helpful?
What can we do to improve the information ?