Technical FAQs

Ask a Question

How does a MM125MB Manual Circuit Closer function?

The MM125MB is a slider type manual circuit closer accessory. The device will be installed onto the meter socket base. A new cover included with the kit contains a notch that allows the circuit closer accessability below the meter socket.


CTA-ID : 2005712
Was this helpful?
What can we do to improve the information ?