Technical FAQs

Ask a Question

Who provides support for Class 8835 Type SFG and 8849 adjustable speed products?

The 8835 SFG was a drive which used a single SCR to control the votlage applied to an 8849 motor. The devices were single phase 120 to 230 vac devices rated up to 1hp.

These devices were obsoleted in the late 1960s and there is no support or alternative devices for them.

CTA-ID : 2005701
Was this helpful?
What can we do to improve the information ?