Technical FAQs

Ask a Question

Does the ATV11 have the ability to use Modbus serial communications.

No. The ATV11 does not support Modbus communications.

However, The ATV28 drive has a built in RJ45 com port that can use  Modbus RS-485 communications.

See the link for more information on serial communications using the ATV28 drive.


CTA-ID : 2005478
Was this helpful?
What can we do to improve the information ?