Technical FAQs

Ask a Question

What is the part number for the 24 VDC I/O extension card?

There are 2 possibilities:
The VW3A66201T includes AO3 (Analog output 3)
The VW3A66201AT does not include the analog output.
The number VW3A66201 may be printed on the cards. To order, the ``T`` or ``AT`` must be added to the part number.

CTA-ID : 2005473
Was this helpful?
What can we do to improve the information ?