Technical FAQs

Ask a Question

What is the duty cycle of the FAL34070?

Circuit breakers are not rated by duty cycle. UL Endurance: 6000 full load operations and 4000 no load, ON / OFF operations.


CTA-ID : 2005469
Was this helpful?
What can we do to improve the information ?