Technical FAQs

Ask a Question

Which circuit breakers may be used in the PIN-QO plug-in unit?

Issue:
Which circuit breakers may be used in the PIN-QO plug-in unit?

Product Line:
Busway.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
Either the QO or QOxxxH type breakers may be used.


CTA-ID : 2005468
Was this helpful?
What can we do to improve the information ?