Technical FAQs

Ask a Question

What is the ``top of box mounting height`` requirement on the Special Features tab of Product Selectors used for?

The top of box mounting height dimension is used to calculate the length of BOTTOM MOUNTED panel skirts and wireways. If a TOP MOUNTED, panel skirt or wireway is called for, the ``ceiling height`` dimension is also required.

Revised 3/10/04

CTA-ID : 2005464
Was this helpful?
What can we do to improve the information ?