Technical FAQs

Ask a Question

Are the XVP audible sounders adjustable to more than 1 tone?

The XVP has 10 tone selections adjusted via jumper and dB level is adjustable from 70 to 85 dB and has various sound formats such as intermittent, continuous, sawtooth etc.


CTA-ID : 2005909
Was this helpful?
What can we do to improve the information ?