Technical FAQs

Ask a Question

Are the XVB audible sounders adjustable to more than 1 tone?

No. The dB level is adjustable from 70 to 90 dB and the sound is either continuous or intermittent.


CTA-ID : 2005908
Was this helpful?
What can we do to improve the information ?