Technical FAQs

Ask a Question

What is the difference between a QO360-314 and QO360-311.

The -314 and -311 are special magnetic calibrations. -314 is 15 times the handle. The -311 is 12 times the handle rating.


CTA-ID : 2005696
Was this helpful?
What can we do to improve the information ?