Technical FAQs

Ask a Question

Is hinged trim available on QMB panelboards installed in NEMA 1 enclosures?

No. The only option is surface w/ door.


CTA-ID : 2005688
Was this helpful?
What can we do to improve the information ?