Technical FAQs

Ask a Question

Is Type 1 door-in-door available on QMB panelboards?

Issue:
Hinged door option

Product Line:
Panelboards

Environment:
QMB

Cause:
Exterior trim 

Resolution:
No. The only option is surface with door.


CTA-ID : 2005689
Was this helpful?
What can we do to improve the information ?