Technical FAQs

Ask a Question

What is the part number for field installation of Start-Stop control station for LE1UD IEC Enclosed Starters?

LA9A Insta-Kit, for kits with additional options such as pilot lights see IEC Controls Insta-Kit section of the current Digest.

CTA-ID : 674
Was this helpful?
What can we do to improve the information ?