Technical FAQs

Ask a Question

Are generator panels available with greater mains ratings than available in the QO48M30DSGP (30 ampere) or QO48M60DSGP (60 ampere)?

No merchanised generator panels are available other that the two noted, However, Manual Transfer Equipment Kits are available for field installation to build a generator panel. Consult the latest Square D Digest, or Digest Plus Selector, available on-line at

CTA-ID : 2006104
Was this helpful?
What can we do to improve the information ?