Technical FAQs

Ask a Question

Does the UL listing on the Homeline load center restrict the types of applications that the load center can be used in?

The Homeline load centers can be used in residential, commercial or industrial applications when applied within its applicable ratings.

CTA-ID : 2005895
Was this helpful?
What can we do to improve the information ?