Technical FAQs

Ask a Question

Are alternate lugs available to accept 3 750kcmil per phase on an NX361200?

Using compression lug kit VC1200NE7 (4) 500 to 750 kcmil Al or 500 kcmil Cu can be used. Requires compression tool VC6FT or VC8.
CVC1200NE7 will accept (4) 500 to 750 kcmil Cu only.

CTA-ID : 2005675
Was this helpful?
What can we do to improve the information ?