Technical FAQs

Ask a Question

What is the wire range for the lugs in a QO2125BNS circuit breaker enclosure?

This device will accept (1) #12-2/0 AWG Aluminum or #14-2/0 AWG Copper conductor per line side phase and neutral. The service ground lug will accept (1) #12-2 AWG Aluminum or #14-2 AWG Copper grounding conductor. See the field installed QO circuit breaker for load side phase lug terminations.


CTA-ID : 2005667
Was this helpful?
What can we do to improve the information ?